EXTENCODER.POSMODULO
Description
Sets/gets the external encoder (EEO) modulo position.
General Information
Type |
R/W |
Units |
1/(2^64) |
Range |
0 to +2^64 - 1 |
Default Value |
0 Counts (off) |
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
---|---|---|---|---|---|
Modbus |
1084 |
Yes | 64 bit | No |
M_01-05-11-000 |